FactoryTalk AssetCentre Inventory Viewer
When you run a backup or backup and compare schedule on an Asset Inventory asset, the Asset
Inventory agent service scans the connected devices and computers on the network and stores
unique identification information about hardware, firmware, and software in the backup data.
You can open the backup data in the
Asset Inventory
window in the FactoryTalk® AssetCentre
desktop client, which shows the scanning result of devices
and associated software in grid view. From FactoryTalk AssetCentre version 15.00.00, you can use the standalone FactoryTalk
AssetCentre Inventory Viewer to view or edit the backup data on any computer without opening
or installing the FactoryTalk AssetCentre desktop client.
IMPORTANT:
The version of this tool must match the version of the FactoryTalk AssetCentre system. For
example, the FactoryTalk AssetCentre Inventory Viewer version 15.00.00 should not be used
with FactoryTalk AssetCentre version 16.00.00. For instructions on how to upgrade this tool
to the latest version, see Upgrade standalone tools in the
FactoryTalk AssetCentre
Installation Guide
.Use the FactoryTalk AssetCentre Inventory Viewer to:
- View the detailed scanning results of hardware, firmware, and software.
- Edit additional information to the scanning results if necessary.
Provide Feedback