Open an Asset Inventory backup file
You can open an Asset Inventory backup file to view or edit the scanning result. Make sure that you have the RAAI file copied to your local computer before attempting to open it.
To open an Asset Inventory backup file with standalone tool
- OnFactoryTalk AssetCentre Inventory Viewer, select
. - Find the RAAI file that you want to view or edit.
- SelectOpen.TIP:You can also modify the default program associated with the RAAI file type, which allows you to open the file without launching the FactoryTalk AssetCentre Inventory Viewer first.
- Right-click the RAAI file, and then selectProperties.
- In theOpens withfiled, selectChange.
- Find and selectFTACInventoryViewerin C:\Program Files (x86)\Rockwell Software\AssetCentre Tools\AssetCentre Inventory Viewer.
Provide Feedback