Change commission date
Commission date is the date on which an equipment, facility, or plant (which is installed, complete, or near completion) is tested to verify if it functions according to its design objectives or specifications. You can change the commission date in the Asset Inventory result by editing the
Commission Date
field. To change the commission date
- On theDevicestab in theFactoryTalk AssetCentre Inventory Viewerwindow, select the dropdown arrow
in the Commission Datecolumn. - Browse the calendar and select the date as needed.TIP:The
button is only available when changes are made to the commission date field. If you want to clear the changes made to additional information, select the
button.
Provide Feedback