Controller Profiles
The Controller Profiles section allows users to add and manage controller IP addresses as
individual profiles. These controllers serve as sources for selecting tags used in
defining state definitions, monitoring on/off tags for training and monitoring a
component, and configuring output controllers for operator notifications. For more
information, refer to the below topics:
Provide Feedback