Configuration Workspace

In the upper-right corner of the page, the gear icon provides access to the following configuration options:
  • General
    : Configure the application parameters.
  • Notifications
    : Set up email notifications.
  • Controller Profiles
    : Manage the controller profiles.
Configurations Workspace
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal