Download UDT

A custom UDT structure is available to enable the controller (PLC) to communicate with FactoryTalk Analytics GuardianAI. Click
Download UDT
to download. The users can import that UDT to a tag inside the required controller, which can be configured in the
Output Controller
section to support operator notifications.
Download UDT
Also the user can download the UDT here: raC_UDT_Itf_GuardianAI.zip
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal