Adding a new Drive and Asset to Monitor

To add a new asset to monitor, the user should complete the four steps summarized in the following diagram.
  1. Add and configure the variable frequency Drive. Supported drives include Powerflex 755, 755TS/TL/TM/TR and 6000T.
  2. Define the Asset to monitor (pump, fan, blower, motor for other asset types).
  3. Configure Training (define the minimum and maximum speed of the application).
  4. Start Training & Monitoring.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal