Configuration Summary
After completing the steps for drive, asset, and training configuration, FactoryTalk
Analytics GuardianAI provides a summary page with final content validation. If any required
field is missing, the configuration step is displayed with a yellow exclamation mark. Once all
fields are completed and validated, the user will be able to click
Finish
to finish the configuration of the new asset.Once user finish the configuration, they are redirected to start training a baseline.
Configuration Summary and Validation

Provide Feedback