Configure Drive
Perform the following steps to configure a new drive:
- On theAsset Overviewsection, clickConfiguration.
- Select the desired folder, clickAdd>New Drive.
- Provide the following details inDrivesection ofConfiguration:
- Select type of drive: Select the required type of drive. One of PowerFlex 755, 755TM, 755TR, 755TL, 755TS, 6000T.
- Name of drive: Provide a unique name for the drive.
- Drive description: Provide a detailed description of the drive. This is optional.
- Drive Path: Provide the drive path.Configure Variable Frequency Drive Parameters
The drive path depends on the network configuration of the drive and the PC hosting FactoryTalk Analytics GuardianAI. If both are on the same network, the drive can be accessible directly via an IP Address. In this scenario, the user can input the drive's IP address.- IP Address example format: 192.168.1.10
The following illustration depicts the PC that hosts FactoryTalk Analytics GuardianAI and the drive existing on the same network location.Network Illustration of Edge PC and Drive on the Same Network
The more likely scenario is the PC that hosts FactoryTalk Analytics GuardianAI is not on the same network layer as the controller. In this case, the user must input the full CIP path mapping from the controller to the drive.- CIP Path format: {BridgeIP}/Backplane/{BridgeModuleSlot}/2/{TargetDriveAddress}CIP Path Example: 11.70.20.214/Backplane/2/2/192.168.1.103
CIP Path Routing Illustration
The following illustration depicts the PC hosting FactoryTalk Analytics GuardianAI on the control network and the variable frequency drive (VFD) on a subnet.Network Illustration of Edge PC on the Control Network and Drive on a Subnet
If there are multiple controller networks to7connect to a drive, the user must input the full CIP path mapping from the controller to the drive as shown below:- CIP Path format for 3 networks: {BridgeIP}/Backplane/{BridgeModuleSlot}/2/{BridgeIP}/Backplane/{BridgeModuleSlot}/2/{TargetDriveAddress}CIP Path Example: 10.91.21.168/Backplane/5/2/10.91.20.4/Backplane/2/2/192.168.1.101
CIP for 3 Networks
- ClickTest Connectionto verify that the drive is connected and FactoryTalk Analytics GuardianAI can successfully establish and validate the connection.
- Click Save. TheDrive Details Updated Successfullymessage displays.
- ClickNextto add the asset details.
Provide Feedback