Configure Asset Training

Perform the following steps to configure Asset training:
  1. Provide the following details in
    Asset
    section of
    Configuration
    :
    • Output Frequency Min (Hz)
      : Minimum VFD command frequency of the application
    • Output Frequency Max (Hz)
      : Maximum VFD command frequency of the application
  2. Provide the following details in
    Advanced Settings
    section:
    • Training Iterations (Default 100)
      : The number of data trends received from the variable frequency drives from FactoryTalk Analytics GuardianAI. A lower value trains faster but generally results in a lower-quality baseline. The recommended value to use is 100 iterations. The expected time taken to train the baseline will be between 11-18 minutes for each half-hertz increment of the operation frequency.
    • Trigger Value Hz (Default Empty)
      : An advanced trigger configured for the drive high-speed trend object. The value set will configure the drive to only send data to FactoryTalk Analytics GuardianAI for training/monitoring when the drive operates at or above the frequency value set for the trigger. This parameter is used for advanced motion-based applications with the variable frequency drive. It will typically not be required when operating FactoryTalk Analytics GuardianAI on pumps, fans, and blowers.
    NOTE: The training performance may be impacted when running FactoryTalk Analytics GuardianAI on Windows via a Linux virtual machine. It is also recommended to place FactoryTalk Analytics GuardianAI as close as possible to the drive application to minimize the number of network hops.
    Configure Training Parameters
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal