Creating an AADvance Project
Create AADvance projects from the
AADvance-Trusted SIS Workstation software®
. A project consists
of hardware platforms called controllers. A project can contain one or more program
organization units (POUs). POUs are programs, functions, or function blocks. POUs are linked
together in a tree-like architecture and can be described using any of Sequential Function
Chart (SFC), Structured Text (ST), Function Block Diagram (FBD), or Ladder Diagram (LD)
programming languages.
TIP:
Regularly save changes made to projects and libraries. Before performing
modifications, save the project to prevent the loss of modified communication
information.
Templates available for AADvance projects:
- Import AADvance Project, enables importing an AADvance project.
- Restore Project from an Archive, enables restoring an AADvance project that was previously archived from a repository inAADvance-Trusted SIS Workstation softwareversion 1.0 orAADvance® Workbench2.1.
- Create Empty Series 9000 Project, enables creating an AADvance project containing one controller.
To start
AADvance-Trusted SIS Workstation software
with the Windows
administrator
privileges required for AADvance projects, right-click the SIS Workstation
Windows
desktop shortcut and select Run as administrator
. Set these properties for projects:
Property | Description |
|---|---|
Comment | Plain text |
Description | Rich text |
Name (Read-only) | Name of the project. Project names are limited to 32 characters beginning with a letter or single underscore followed by letters, digits, and single underscores. The last character for a project name must be a letter or digit; project names cannot end with an underscore character. Reserved words, defined words, or data types such as, elementary, structures, or arrays are not valid names. Use unique names for projects within a directory. |
Password Protected (Read-only) | Indication that the project is protected by a password controlling its access |
Path (Read-only) | Complete path where the project files are stored on the computer. The path is automatically assigned: %USERPROFILE%\Documents\SIS Workstation 1.0\Projects\ProjectName Modify the storage location for projects in the Projects options from the Tools > Options menu. Set a local path for the project location; network paths may cause unexpected results. |
Perform these tasks for projects:
Task | Procedure |
|---|---|
Create an AADvance project |
|
Set properties for a project |
|
Import target definitions |
TIP:
Do not import target definitions.
|
Build a project |
|
Clean a project |
|
Download project code |
TIP:
Avoid downloading an application containing zero POUs or empty POU
bodies.
Build the project code.
|
Control access for projects by setting a password restricting modifications like adding controllers, programs, functions, and function blocks.
Provide Feedback