Archive and Restore Repository Projects
Archive projects contained in a repository and restore projects that were previously archived. Archiving a repository project means compressing the content of a project into a *.vsc file. Either archive the complete version of a project, including the modification history and all comments, or archive the latest version of a project checked into a repository. Then restore the archived file in another repository. The archived file can then be restored in another repository. Performing updates or connecting to controllers is unavailable after restoring a project archived at the latest version.
TIP:
To reduce the time taken to perform archive and restore
operations, have a different repository folder for each project.
Restore AADvance projects archived with
AADvance-Trusted SIS Workstation software®
version 1.1 or AADvance® Workbench
version 2.1. Projects archived from AADvance-Trusted SIS Workstation software
version 1.1 cannot be restored in previous versions of the AADvance Workbench
or AADvance-Trusted SIS Workstation software
.
TIP:
Before archiving a project at the latest version, it is
recommended to label the version of the project, ensuring the version control history
displays the expected description after project restoration.
To archive and restore repository projects
To start
AADvance-Trusted SIS Workstation software
with the Windows
administrator privileges required for AADvance projects, right-click the SIS Workstation
Windows
desktop shortcut and select Run as administrator
. Then, continue with one of the procedures in this table. Task | Procedure |
|---|---|
Archive a repository project |
|
Restore a repository project | Restore AADvance projects archived with AADvance-Trusted SIS Workstation software version 1.1 or AADvance Workbench version 2.1.
TIP:
Before restoring the project, limit the
Projects location path length to 70 characters. Setting a longer path may exceed
the maximum length of 260 characters supported by
Windows
operating systems.When setting the project location, specify a local path;
network paths may cause unexpected results.
|
Restore multiple versions of the same project | When restoring multiple versions of the same project, the AADvance project archive significantly increases in size.
|
From the
Application View
, perform version control operations for all elements. From the Communication View
and Equipment View
, perform version control operations for projects and controllers.Provide Feedback