Accessing Repository Projects
While working with AADvance controllers, access projects stored in a repository. When multiple computers need to access the same project, it is recommended to use a repository in a shared folder. This preferred method enables different users to check out and modify the project while ensuring a complete modification history. Only one user can check out a project element at any given time.
When only using a locally stored repository, the may require transferring the storage location of the repository to another computer. Transferring a repository also transfers all of the projects contained within the repository folder. Needing to transfer the storage location of the repository occurs when upgrading to a new computer or permanently changing workstation. Keep only one instance of the repository folder.
When needing to access a specific project on a computer other than the one storing the local repository folder, it is recommended to archive the project and then restore the *.vsc file in the local repository folder of the other computer.
TIP:
Modification history is retained when restoring the
project.
Provide Feedback