To access a repository in a shared folder
Accessing a repository in a shared folder enables different users to check out and modify the project while ensuring a complete modification history. Only one user can check out a project element at any given time.
IMPORTANT:
A project with the same name as a project saved
in the projects directory cannot be opened; delete the local copy before opening the
project.
To access a repository in a shared folder
- From theFilemenu, point toVersion Control, and then clickSelect Repository.
- In theSelect Repositorydialog box, clickBrowseto locate the shared folder, and then clickOK.
- For all required computers, ensure theAADvance-Trusted SIS Workstation software®uses the repository located in the shared folder.
Provide Feedback