To transfer a repository to another computer

Transfer the storage location of the repository to another computer. Transferring a repository also transfers all of the projects contained within the repository folder. Keep only one instance of the repository folder.
IMPORTANT: A project with the same name as a project saved in the projects directory cannot be opened; delete the local copy before opening the project.
To transfer to a repository to another computer
  1. Transfer the repository folder to another computer.
    TIP: Make sure to remove the repository folder located on the original computer.
  2. On the other computer, open the
    AADvance-Trusted SIS Workstation software®
    and then from the
    File
    menu, point to
    Version Control
    , and then click
    Select Repository
    .
  3. In the
    Select Repository
    dialog box, click
    Browse
    to locate the transferred repository folder, and then click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal