Labeling a Version

Label a version of a project or an element for reference in the repository. The label is also applied to all sub-elements of the latest version checked in to the repository.
From the
Application View
, perform version control operations for all elements. From the
Communication View
and
Equipment View
, perform version control operations for projects and controllers.
To label a version
  1. From the required view, select the project or element for which to apply a label.
  2. From the
    File
    menu, point to
    Version Control
    , and then click
    Label
    .
  3. In the
    Add Label
    dialog box, enter the text to display as the label in the version control history, and then click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal