Check In Elements to Version Control

Check in AADvance elements like projects, libraries, controllers, programs, functions, and function blocks to a repository. Check in elements to manage the changing versions of elements and retrieve previous versions. Also add elements to previously checked in projects.
Prerequisites:
  • The project contains no empty structure types, array types, user-defined function block POU bodies, or variables.
  • The project contains no child SFC program organization units (POUs) for Sequential SFC Chart (SFC). Use only SFC programs and function blocks.
When creating a project, all elements are automatically checked in to the repository.
Use a recursive check in to check in elements with sub-elements. Also choose to keep elements checked out following a check-in. Recursive operations do not modify elements locked while checked out by other users.
IMPORTANT: Immediately check in modifications after deleting or renaming elements to ensure that subsequent deleting and renaming are possible.
Perform version control operations for all elements from the
Application View
. Perform version control operations for projects and controllers from the
Communication View
and
Equipment View
.
To add or check in elements to version control
  1. From the required view, select the element to add or check in to the repository.
  2. From the
    File
    menu, point to
    Version Control
    , and then click
    Check In
    .
  3. In the
    Check In
    dialog box, indicate whether to perform a recursive check in and whether to keep the elements checked out following the check-in, and then click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal