Checking Out Elements from Version Control

Check out AADvance elements like projects, libraries, controllers, programs, functions, and function blocks from a repository. Checking out provides exclusive access when modifying these elements. When modifying elements that are checked in, these elements are automatically checked out when not checked out by another other user
When creating a project, all elements are automatically checked in to the repository.
When checking out elements with sub-elements, perform a recursive check out which includes checking out sub-elements. When performing recursive operations, elements locked while checked out by other users are not modified.
From the
Application View
, perform version control operations for all elements. From the
Communication View
and
Equipment View
, perform version control operations for projects and controllers.
To check out elements from version control
  1. From the
    Application View
    , select the project or element to check out from the repository.
  2. From the
    File
    menu, point to
    Version Control
    , and then click
    Check Out
    .
  3. In the
    Check Out
    dialog box, indicate whether to perform a recursive check out including all sub-elements, and then click
    OK
    .
    The elements are checked out from the repository and display with the unlocked icon in the
    Application View
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal