Import an AADvance Project
Import existing projects created using any version of the
AADvance-Trusted SIS Workstation software®
or AADvance® Workbench
.
IMPORTANT:
To import a project with its library using
AADvance-Trusted SIS Workstation software
, see Import an AADvance Project with Library.To import an AADvance project
- To startAADvance-Trusted SIS Workstation softwarewith theWindowsadministrator privileges required for AADvance projects, right-click theSIS WorkstationWindowsdesktop shortcut and then selectRun as administrator.
- From theFilemenu, clickNew Project.....
- In theNew Projectdialog box, in theAADvancetab, clickImportin theProject Typeslist.
- In theTemplateslist, clickImport AADvance Project.
- Specify a name for the project, and then clickBrowseto select the database path.
- In theSelect Database Filedialog box, locate and select the project database file (*.mdb or *.accdb), and then clickOpen.
- A message may display asking to update the database to the current version. Note that after updating the database, the project can no longer be opened in a previous version ofAADvance Workbench. To continue the importation process, clickOK.
- In theNew Projectdialog box, clickOK.The imported AADvance project is available for use inAADvance-Trusted SIS Workstation software.
- From theBuildmenu, selectClean All.
Provide Feedback