Import an AADvance Project with Library

Import existing projects with their library created using any version of the
AADvance-Trusted SIS Workstation software®
or
AADvance® Workbench
.
To import an AADvance project with its library
  1. Before importing the original project, rename the library folder that contains the MDB file used by this project.
  2. Import the project. For more information refer to Import an AADvance Project.
    The dialog box appears.
    1. If you are warned there is a Project Missing Files, select
      Yes
      .
    2. If you are asked to update the database, select
      Ok
      .
  3. Select the project in the Application View and select
    File > Version Control > Check Out
    .
    The Check-Out Confirmation dialog box appears.
  4. Select
    OK
    .
  5. Add a New Library. For more information refer to AADvance Libraries.
    The Security Password dialog box may appear. If it does, enter the password of the library again and select
    OK
    .
  6. Select the project in the Application View and select
    File > Version Control > Check In
    .
    The Check-In Confirmation dialog box appears.
  7. Select
    OK
    .
  8. Select
    FILE> Save All
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal