Setting Project Access Control
For project security, set access control using a password for projects, controllers, program organization units (POUs), libraries, and library functions and function blocks. Password definitions are limited to eight characters and can consist of letters and digits. Enter the password to open a password-protected project. Project sub-elements, can have their own level of access control. Example: a POU with its own password remains locked and cannot be modified without entering its password.
Since POUs are encrypted, password definitions must be retained.
In the
Application View
, the following indicates the security state for elements:
Indicates that a lock is applied to the elementWhen opening a project with password-protected elements, there is a prompt to enter the password once for each element. Password-protected elements have these modification restrictions:
Password-Protected Element | Modification Restrictions |
|---|---|
Project | Opening the project |
Controller | Adding, editing, and deleting a program, modifying the communication protocols, modifying the system type and controller properties, wiring variables, and adding, editing, and deleting I/O modules. |
Program | Viewing the program |
Library | Adding, editing, and deleting a library function or function block |
Library Function | Viewing the function |
Library Function Block | Viewing the function block |
Edit existing passwords for projects and project sub-elements. Also remove existing passwords. When copying, pasting, importing, and exporting elements with access control, password definitions are retained.
Task | Procedure |
|---|---|
Set a password |
|
Edit a password |
|
Remove a password |
|
Provide Feedback