Opening an AADvance Project

When opening a project, choose from projects available from the current version control repository. The available projects also lists the recently opened projects.
To open an AADvance Project
  1. To start
    AADvance-Trusted SIS Workstation software
    with the
    Windows
    administrator privileges required for AADvance projects, right-click the
    SIS Workstation
    Windows
    desktop shortcut and select
    Run as administrator
    .
  2. From the
    File
    menu, click
    Open Project
    ... (or press
    Ctrl+Shift+O
    ).
  3. In the
    Open Project
    dialog box, select the required project, and then click OK.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal