Setting Target Access Control
For controller security, set access control by defining a password for the target AADvance controller. Password definitions are limited to eight characters and can consist of letters, digits, and symbols. Target access control prevents the connection of all IXL clients not having the password for the target controller. Users having the password can attach the target to controllers in different projects.
TIP:
The password definitions for controller targets are
saved on target systems.
Targets with passwords are protected from:
- Stopping the application from theAADvance-Trusted SIS Workstation software®
- Downloading an application
- Updating an application
- Locking a variable
- Modifying the value of a variable
Existing passwords for targets can be edited. Existing passwords for target controllers can be removed. When setting, editing, and deleting the password for a controller target, the attached target must be running.
Task | Procedure |
|---|---|
Set a password for a target |
|
Edit a password for a target |
|
Remove a password for a target |
|
Provide Feedback