Upload the SYSTEM.INI file from the TMR Processor
Upload the SYSTEM.INI file from the
Trusted®
TMR Processor. The SYSTEM.INI file transmits in packets of data.Prerequisite
- Enter design mode.
To upload the SYSTEM.INI file from the TMR Processor
- From theSystem Configuration Tool, click
Read from TMR Processoror selectFile>Read from TMR Processor. The TX LED in theCommunications in progresswindow flashes as each packet of data uploads. The RX flashes to indicate the successful upload of a packet. - After the successful completion of the upload, in theCommunications in progresswindow, clickOK.TIP: After successfully downloading of the new or modified SYSTEM.INI, either reboot theTrusted®TMR Processor to implement the file, or stop then start the application.
Provide Feedback