Generating the SYSTEM.INI file
After configuring the required information in the
System Configuration Tool
, generate the SYSTEM.INI file. After generating the SYSTEM.INI file, view the current contents of the file in the buffer. Modify the text font and text colors that display in the SYSTEM.INI and associate all *.ini files with the current application.
Also generate a diagram of the
Trusted®
system from the SYSTEM.INI file. Regenerating the graphic from the INI buffer updates the display of the System Layout
displayed in the System Configuration Tool
. Print the SYSTEM.INI text file and diagram.
Task | Procedure |
|---|---|
Generate the SYSTEM.INI file |
|
Display the contents of the SYSTEM.INI file |
|
Generate the SYSTEM.INI file diagram |
|
Print the SYSTEM.INI |
|
Provide Feedback
.
.
.