Configuring the SYSTEM.INI File

The SYSTEM.INI text file configures the operational parameters of a
Trusted®
controller. To configure the SYSTEM.INI file, you need to have created all required system templates. You also need to configure the communication port to download the SYSTEM.INI file to the TMR Processor. To configure the SYSTEM.INI file, you need to do the following:
  • Configure the
    Trusted
    TMR Processor
  • Assigning modules and adding the expander chassis
  • Configuring I/O modules
  • Configure the 8151 Communications Interface module
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal