Configuring the Trusted TMR Processor
Trusted
TMR ProcessorAccess the module to configure the 8110 TMR Processor.
TIP:
For information on configuring the
Trusted®
TMR Processor, refer to the T8110B Trusted
TMR Processor product description.To access the 8110 TMR Processor configuration
- From theSystem Configuration Tool, in theSystem Layout, click the 8110 TMR Processor module in the first slot.

Provide Feedback