Download the SYSTEM.INI file to the TMR Processor
Download the SYSTEM.INI file to the
Trusted
TMR Processor to configure the Trusted®
system. The SYSTEM.INI file transmits in packets of data. Prerequisites
- Configure the communication port.
- Set the enable key switch on the TMR Processor toMaintain.
- Enter design mode.
To download the SYSTEM.INI file to the TMR Processor
- From theSystem Configuration Tool, click
Write to TMR Processoror selectFile > Write to TMR Processor. The TX LED in theCommunications in progresswindow flashes as each packet of data downloads. The RX flashes to indicate the successful download of a packet. - After the successful completion of the download, in theCommunications in progresswindow, clickOK.TIP: After downloading the new or modified SYSTEM.INI, either reboot theTrusted®TMR Processor to implement the file, or stop and then start the application.
Provide Feedback