User-defined libraries
User-defined libraries promote reuse, streamline workflows, and create
consistency by allowing you to standardize objects. Use user-defined libraries to
customize the separation and organization of groups of objects in a project.
User-defined libraries are distinct from the
Project library
. You
can create multiple user-defined libraries in a project, share and then import those
user-defined libraries into other projects, and delete user-defined libraries from the
project. You cannot delete or share the Project library
outside of the
project.Create a user-defined library to curate reusable content, such as Add-On Instructions,
Smart Objects, and Data Types. Once created, user-defined libraries that you create
appear in the
User-defined libraries
folder of the
Library
explorer.Provide Feedback