Import a shared library to use the object definitions in that library in your
project. Importing a shared library prevents having to recreate objects that exist in another
library. Two versions of the same library cannot exist in a
FactoryTalk®
Design Studio™
project.
In the explorer bar, select
Library
and then right-click the
User-defined
libraries
and then select
Import user-defined
library
.
TIP:
To import a shared library, you can also select
File > Import > User-defined library
and search for the
library.
In
Import user-defined library
, search for or navigate to the
library to import.
(optional) To delete a shared library that you no longer need from the shared library
location of your organization, select the row of the shared library. select
Delete
, and then select
Delete
again to
confirm the deletion.
TIP:
The ability to delete a shared library depends on
your assigned user role:
Guest. Cannot delete a shared library.
Admin. Can delete any library shared within the organization.
Engineer. Can only delete libraries that they share.
TIP:
You cannot undo the deletion of a shared library.
Select the library to import and select
Import
.
NOTE:
If you try to import a library that already exists in your
project, you are prompted to select
Apply
to delete the local
version of the library and import the new version.