Share a user-defined library

Share a user-defined library so that its objects can be used across projects and teams in your organization. Users can then import the library to use its objects in their projects.
You can share different versions of the same user-defined library. By default, you can only share a user-defined library if you have the Engineer role or a custom role defined with the Share User-Defined Library permission. The Library is shared to your organization and is available to import from a
FactoryTalk Design Studio
project.
Create a user-defined library
To share a user-defined library
  1. In the explorer bar, select Library icon
    Library
    .
  2. Expand
    User-defined libraries
    .
  3. Right-click the library to share and select
    Share user-defined library
    .
    Factory Talk Design Studio validates the user-defined library to share.
    TIP: Selecting a library in
    Share user-defined library
    displays the three most recently shared versions of the library as well as the local version or latest version to share.
  4. In
    Share user-defined library
    , complete:
    • Version
      . Enter major and minor version numbers for the library that you are sharing. If you have shared the library before and have now made changes to the library, enter a new version for the library.
    • Release note
      . Enter a description of the contents or changes in the library that you are sharing.
  5. Select
    Share
    .
    The Library is shared to your organization and is available to import from a
    FactoryTalk Design Studio
    project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal