IntelliCENTER Dashboard components

The
IntelliCenter Dashboard
contains the following components:
Component
Decription
Option to open the IntelliCENTER dashboard at the bottom of the IntelliCENTER explorer
MCC lineups in the IntelliCENTER Dashboard
Option to
Import new lineup
. You can import either the pre-shipment or post-shipment dataset purchased with your IntelliCENTER Motor Control Center.
Option to
Export lineup
. Export a lineup to use the lineup in the local installation of IntelliCENTER. See Export an MCC lineup.
Option to
Edit Network Path
. The network path specifies the target network for status monitoring in an IntelliCENTER lineup.
Status of the MCC lineup. Status appears when you monitor a lineup.
Toggle to turn on and off monitoring of an MCC lineup.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal