Unit and device status indicators
The Overall Unit Status indicator appears only when a unit when a device within the unit
has either a Warning, Fault, or Communication loss status.
A secondary status icon appears on the unit and represents the most significant status
within the unit. Status icons listed in ascending order of significance include:
Device & Unit Secondary Status Icons | Description | Overall Unit Status Icon |
|---|---|---|
Communication not supported with device | No icon | |
Ready | No icon | |
Running | No icon | |
Warning | ||
Fault | ||
Communication Loss |
Provide Feedback