Device status monitoring
When status monitoring is enabled, IntelliCENTER communicates with supported
devices to determine if a device is in the Ready, Running, Warning, Fault or
Communication Loss state.
Status monitoring requires the following entitlements:
- FactoryTalk Remote with Pro entitlement
- FactoryTalk Design Studio Core entitlement
You can monitor the status of:
- Lineups. Lineup level status indicates the most significant status within the entire lineup. View lineup level status from the IntelliCENTER Dashboard.
- Units. Unit level status indicates the most significant status within the unit. View unit level status inElevationview or from the unit profile.
- Devices. Individual device status is viewed through the unit tooltip inElevationview. You can also expand the IntelliCENTER explorer to navigate to the device level or view the unit profile.
Provide Feedback