Start and stop status monitoring

Monitor devices by starting and stopping monitoring from the IntelliCENTER explorer, Elevation view, and the IntelliCENTER dashboard. All network paths must be set to monitor devices. If you select
Start Status Monitoring
before all network paths are set,
Set Network Path
opens for you to set network paths.
  1. On the explorer bar, select Devices Icon
    Devices
    .
  2. Select
    IntelliCENTER
    .
  3. In the
    IntelliCENTER
    explorer, right-click a lineup and select
    Start Status Monitoring
    or to stop monitoring already in progress, select
    Stop Status Monitoring
    .
    TIP: To monitor devices from
    Elevation
    view, double-click the the lineup name and then in
    Elevation view
    , right-click blank space and then select
    Start Status Monitoring
    .
    TIP: To monitor devices from the IntelliCENTER Dashboard, select
    IntelliCENTER Dashboard
    and then next to the lineup name toggle
    Start Status Monitoring
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal