Set network paths
The network path specifies the target network for status monitoring in an IntelliCENTER
lineup. You must provide all network paths within a lineup before the lineup starts status
monitoring. After creating network paths, you can edit the network paths on the
Edit
Network Paths
tab.- On the explorer bar, select
Devices. - SelectIntelliCENTER.
- In theIntelliCENTERexplorer, right-click the lineup and selectSet Network Path.TIP: To set a network path fromElevationview, right-click a blank space and selectSet Network Path.TIP: To set a network path from theIntelliCENTER Dashboard, at the bottom of theIntelliCENTERexplorer, selectIntelliCENTER Dashboard, right-click a lineup, and then selectSet Network Path.
- InSet Network Path, select a network and either paste the network path orBrowseto a path.TIP: To clear a network path, selectDelete.
- To start monitoring for the lineup, selectStart Status Monitoring.TIP: To start status monitoring, all network paths must be set. If you do not want to start status monitoring, selectSave and Closeto save the network paths and continue working.TIP: To communicate with the controller, Add a VPN driver.
Set Network Path
changes to
Edit Network Path
.
Provide Feedback