Configure Internet Explorer for FactoryTalk Historian ME
In this section, you will learn how to configure Internet Explorer to work with FactoryTalk Historian ME websites.
TIP:
Support for Internet Explorer may be removed in a future release. Series C modules support more modern web browsers like Chrome and Edge.
The following browsers are supported:
- Microsoft®Internet Explorer®11
The following operating systems are supported:
- Windows®10
- Windows Server®2019
- Windows Server2016
- Windows Server2012TIP:This section has been prepared assuming that you access the module by typing its IP address in the browser. If you access the module by typing the Fully Qualified Domain Name (FQDN) of the module in the browser, follow the instructions, and type the FQDN instead of the IP address.
Provide Feedback