Verify the certificate
You can verify the current certificate used by FactoryTalk Historian ME websites in two ways:
- On the security report of the web browser.It is a recommended method to verify the certificate. This report provides detailed information on both the self-signed certificate and the CA certificate.For details, see Verify the certificate on the security report.
- On theSystem Securitypage of the Historian website.This page provides basic information about the self-signed certificate only, and does not provide any details on the CA certificate.For details, see Verify the certificate on the System Security page.
Provide Feedback