Verify the certificate on the security report

To verify the certificate details on the security report
  1. Open the FactoryTalk Historian ME website using the IP address of the module.
  2. Click the padlock icon padlock located to the right of the address field in Internet Explorer.
    The
    Website Identification
    dialog box appears. This is the security report for the webpage.
  3. Click
    View certificates
    .
    The
    Certificate
    dialog box appears.
  4. On the
    General
    tab, review the following information:
    • Issued to
      By default, the certificate is issued to the IP address of the ME module.
    • Issued by
      The same as
      Issued to
      .
    • Valid from - to:
      The validity date of the certificate.
      The certificate is valid for 5 years.
      On the
      General tab
      , only the date (without the time) is displayed. You can see both the date and time on the
      Details
      tab.
      The
      Valid from
      value is not only the start date and time of the certificate's validity period, but also the date and time the certificate was created.
      The date and time change each time you renew the certificate on the
      System Security
      page.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal