Enable TLS

The FactoryTalk Historian ME website requires TLS 1.2. Make sure that TLS 1.2 is enabled.
To enable TLS
  1. On the
    Tools
    menu, click
    Internet Options
    .
    The
    Internet Options
    dialog box appears.
    TIP:
    If the top menu is not visible, press the left Alt key on your keyboard to bring up the top menu.
  2. Click the
    Advanced
    tab, and then under
    Settings
    select the following check boxes:
    • Use TLS 1.0
    • Use TLS 1.1
    • Use TLS 1.2
  3. For security reasons, clear the following check boxes:
    • Use SSL 2.0
    • Use SSL 3.0
  4. Click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal