Enable Compatibility View

To enable Compatibility View
  1. Open the FactoryTalk Historian ME website using the IP address of the module.
  2. On the
    Tools
    menu, click
    Compatibility View settings
    .
    The
    Compatibility View Settings
    dialog box appears.
    TIP:
    If the top menu is not visible, press the left Alt key on your keyboard to bring up the top menu.
  3. Verify that in the
    Add this website
    text box there is the IP address of your module site, and then click
    Add
    .
    TIP:
    If you access the website by typing the hostname or DNS name of the module, make sure that they are set in the text box.
  4. Click
    Close
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal