Enable the XML DOM Document add-on

The FactoryTalk Historian ME website requires the Microsoft XML DOM Document add-on to communicate with the module and send data. Make sure that the add-on is installed and enabled.
To enable the XML DOM Document add-on
  1. On the
    Tools
    menu, click
    Manage add-ons
    .
    The
    Manage Add-ons
    dialog box appears.
    TIP:
    If the top menu is not visible, press the left Alt key on your keyboard to bring up the top menu.
  2. Under
    Microsoft Corporation
    , verify that all XML DOM Document add-ons are enabled.
  3. If the add-ons are disabled, under
    Show
    , select
    All add-ons
    .
  4. Under
    Microsoft Corporation
    , click each XML DOM Document add-on, and then click
    Enable
    .
  5. Click
    Close
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal