Transfer data to FactoryTalk Historian SE or PI servers
Use the data transfer to transfer the data collected by your FactoryTalk Historian ME to a FactoryTalk Historian SE or PI server. You can transfer data to a single FactoryTalk Historian SE or PI server. Server collectives are not supported.
Once you have started the data transfer and selected the data points to be transferred to your FactoryTalk Historian SE or PI server, you can check the transferred points in the System Management Tools.
To visualize the data transfer, you can create a trend in Microsoft Excel using the FactoryTalk Historian DataLink Add-in. For details, see Create trends visualizing the data transfer.
Provide Feedback