Stop the data transfer

To stop the data transfer
  1. Click the
    Configure Historian
    tab, and then click
    Data Transfer
    .
  2. Under
    Data Transfer Parameters
    , click
    Stop
    .
    The status changes from
    Running
    to
    Stopped
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal