View the data transfer information
To view the data transfer information
- Click theConfigure Historiantab, and then clickData Transfer Points.
The
Data Transfer Points
page provides the following information related to the data transfer service on both the FactoryTalk Historian SE or PI server and the Historian module:Information on the FactoryTalk Historian SE or PI server
FactoryTalk Historian SE server item | PI server item | Description |
|---|---|---|
Current Time | The time on the FactoryTalk Historian SE or PI server. | |
Time Offset | The time difference in seconds between the FactoryTalk Historian SE or PI server and the FactoryTalk Historian ME times. | |
FTHSE Licensed Points | - | The number of points that have been assigned to the FTMS point source on FactoryTalk Historian SE. It is based on the currently active license for FactoryTalk Historian SE and is an indication of the number of FactoryTalk Historian ME points that can be transferred to FactoryTalk Historian SE. |
- | Total Licensed Points | The number of points that have been assigned to the PI server. It is an indication of the number of FactoryTalk Historian ME points that can be transferred to the PI server. |
"FTMS" Points Available | Available License Points | The total number of points assigned by the license minus the number of points that are already being transferred to the FactoryTalk Historian SE or PI server. The value may not get updated immediately because it takes approximately fifteen minutes to update the FactoryTalk Historian SE or PI server. |
Information on the FactoryTalk Historian ME module
The section on the Historian module provides the following information:
- The number of data points selected.
- The number of data points newly added to the data transfer.
- The status of the auto transfer mode.
Provide Feedback