View data transfer statistics

The data transfer service records performance statistics that determine the connection reliability. You can use the statistics to refine the data transfer configuration.
The
Data Transfer Statistics
section of the page displays the following information:
Item
Description
Transfer Rate
The number of retrieved events divided by the number of minutes spent on retrieving events sent to the FactoryTalk Historian SE or PI server.
Successful Attempt Rate
The number of attempts to transfer data to the FactoryTalk Historian SE or PI server per hour.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal