Remove points from data transfer
To remove points from the data transfer
- Click theConfigure Historiantab, and then clickData Transfer Points.
- UnderData Transfer Points, type the search criteria, and then clickSearch.The search results are displayed in the table.
- Clear the checkbox next to each data point that you want to remove from the data transfer.If you want to remove all the data points listed, clear theAll/Nonecheckbox at the bottom of the table.
- ClickSave.
- ClickOK.The outcome of the operation is indicated with a message displayed at the top of the page:INFO: Save operation successful.TIP:This way you only remove the data points from the data transfer service. If you want to remove the data points from the FactoryTalk Historian SE or PI server (for example, in order to free some licenses), you must delete the points on the FactoryTalk Historian SE or PI server.
Provide Feedback