System statistics

To open the
System Statistics
page, click System Statistics
on the Home
tab.Choose this option | To display |
|---|---|
Network Manager | The network management statistics. See Network manager. |
Snapshot and Archive | The snapshot and archive statistics. See Snapshot and archive. |
Archive Files | The archive file statistics. See Archive files. |
The information available on this page may be helpful when troubleshooting any issues with your module.
TIP:
For details on sorting and viewing information in tables, see Change views.
Provide Feedback