View the module information
The module information is displayed on the following pages of the
Home
tab:- Module IdentitySee Module identity.
- System UtilizationSee System utilization.
- System StatisticsSee System statistics.
Additionally, there is also the System status section in the lower-left corner of every page of the web client.
Provide Feedback