System utilization

System utilization
To open the
System Utilization
page, click
System Utilization
on the
Home
tab.
The page displays the following information:
This item
Displays
CPU and Processes
The current percent of the CPU in use and the processes currently running.
Note:
The CPU usage percent listed in the
System status
section (see System status) may display a different percent than the percentage listed in the
CPU and Processes
section in the main window. This is because the CPU usage listed in the
System Status
section is updated periodically while the CPU Usage information displayed in the main window is static. It does not change once the page is loaded.
RAM
The memory usage of the module.
Ethernet Statistics
The total amount of data sent and received by the module through the network.
Storage (NAND)
The total storage space used and available on the installed flash drive. This section also displays the total number of archive files and how many of them are free, as well as the archive file size.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal